Honeywell Transportation Systems

11.01.2016
  • Print
  • All Press Releases >

Garrett by Honeywell Unveils New Reverse Rotation Turbochargers

Garrett Performance Parts responds to demand for twin turbo setup option

LAS VEGAS, Oct. 31, 2016 — Honeywell (NYSE: HON) today announced the Nov. 1, 2016, availability of select reverse rotation turbochargers for fabricators and installers seeking an option for symmetrical twin turbo setups and eliminating the need for extra tubing.

Turbo

A GTX3076R reverse rotation turbo

The reverse rotation design allows for more aesthetically pleasing visual symmetry best suited for v-block shaped engines. The new design is engineered for the compressor wheel to rotate counterclockwise thereby pointing the housing outlet in the opposite direction from a standard rotation turbocharger.

“It creates the visual symmetry of a ‘left shoe, right shoe’ appearance that really works well with v-shaped engines for our enthusiast customers,” said, Eric Fraysse Aftermarket vice president and general manager at Honeywell Transportation Systems. “While there are workarounds within the industry to address this preferred setup, these Garrett turbos have been designed and engineered to work seamlessly without compromising performance.”

The reverse rotation turbos are available for select GTX Turbochargers (GTX3071R, 3076R, 3576R, 3582R) and in addition to being brand new, these turbos eliminate the need for additional fabricated piping by feeding directly into the intake manifold. The result also creates a more efficient mirrored setup with equidistant exhaust flow between the two turbochargers.

The reverse rotation turbos feature the new Garrett GTX Series Gen II compressor wheels, as well as other GTX Gen II standard features including water-cooled center housing rotating assemblies, ceramic ball bearings for additional responsiveness, new high-flow compressor housings, a fully machined speed sensor port for enthusiasts that are interested in data acquisition (Garrett speed sensor sold separately). Several unique turbine housing options are also available for each size to fine tune power for bottom end or top end performance.

Honeywell provides reverse rotation turbochargers for some single-unit, factory installed original equipment applications including that used with the current Ford 2.3L EcoBoost engine available in the Ford Mustang.

 

Supporting Resources

 

About Honeywell Aerospace

Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft, and its turbochargers are used by nearly every automaker and truck manufacturer around the world. The Aerospace business unit develops innovative solutions for more fuel efficient automobiles and airplanes, more direct and on-time flights, safer flying and runway traffic, along with aircraft engines, cockpit and cabin electronics, wireless connectivity services, logistics and more. The business delivers safer, faster, and more efficient and comfortable transportation-related experiences worldwide. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero and @Honeywell_Turbo.

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes, and industry; turbochargers; and performance materials.  For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

 

This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.